Hello,
I am looking at the LM5017 and the high Vin(max) is ideal but I am concerned about the relatively high 9V Vin(min). I did notice in the datasheet that the internal UVLO threshold for Vcc is only 4.5V. What would happen if I use the UVLO pin to set a threshold of only 6V? Would the part attempt to operate once Vin is high enough (but still below 9V)? My Vout is set to 5V and I am not guaranteed a Vin as high as 9V in my system.
Thanks,
Dave