Hello,
I successfully used TPS5450-Q1 and TPS5430-Q1 circuits to provide +5V from a 14V battery voltage.
However, I need to understand and deepen the behavior of the chopper in a mode of failure of the bootstrap capacitor ( pin N°1 BOOT).
What is the behavior of the TPS5450 in case of low voltage at the terminals of this capacitor (BOOT / PH), with a stable 12V at VIN pin ?
The high-side mosfet could have a thermal runaway before the thermal protection could be active ?
Is there any under-voltage protection on BOOT pin ( Vin = 12v) ?
Thanks in advance for your answering.