Hi,
I was wondering what was the best method to turn the LM5008 off with out using a mechanical switch which is what is shown in the datasheet.
The Ron (pin6) needs to be pulled low (below 1.5V i think) and then the device turns off.
During operation this pin is used to set the switching frequency.
I can currently only see using a NPN transistor to pull that in down but that means i need something to power the base of the transistor continually. This is not obvious consideringthe wide input voltage supported by the LM5008 (12V to ~90V)
Is there an application note with recommended circuitry to consume the least amount of power while off?
Regards,
Alexis