This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950 spreadsheet possible issue

Other Parts Discussed in Thread: UCC28950

Hello there.

I'm designing a DC/DC converter using the UCC28950. The specifications os the power supply are:

Vin = 390Vdc (PFC)
Vout = 48V
Iout = 21A

I was using the the spreadsheet avaliable in the following link:
http://www.ti.com/litv/zip/sluc222b

But, I believe it has a little issue. In the tab called "Design Information" rolling the sheet down, after the graphic, the resistor called RDELEF must be defined more the once. It must bemn defined in the follwowing places:
"Setting AF and BE..."
"Setting Minimum on Time"
"Setup PWM..."
"Setup Slope Compensation"

If thats not an error which value I must consider?