In the LM3429 datra sheet page 10, section "CURRENT SENSE/CURRENT LIMIT" it is mentioned that there are two methods to sense transistor current. It goes on to detail method two, using a resistor in series with the main MOSFET and connecting the IS pin to the source. But method 1 is not detailed, it's only mentioned that the Rds(on) is used as the current sense resistance.
So, what's the formula? Would it be:
I(lim) = 0.245/Rds(on) ?
(also is there any way to get web-bench to use this topology)
looks like the same question would apply to the LM3421 etc.