This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NEED INFORMATION- V62/03629-02YE

Hi Can you please provide the following information for the V62/03629-02YE  Part ?

1. Junction Temperature Max (Tj Max)

 2. Typical Power dissipation (Pd typ)

3. Maximum Power dissipation (Pd max)

4. Thermal Resistance Junction to Ambient (Theta JA

5. Thermal Resistance Junction to Board (Theta JB)

6. Thermal Resistance Junction to Case (Theta JC)

7. Weight

Regards,

Jayakumara K

jayakumara.krishnasetty@honeywell.com

Tel:   +91-80-26588360   Extn: 50116

  • Hi Jayakumara,

    Searching this in the search toolbar yields the TPS3307-33EP.

    1. Please see the abs max rating on page 4 of the datasheet: 150 degC.

    2. Typical Power dissipation depends on operating conditions: Pd is approximately VDD*IDD

    3. This will depend on the ambient temperature and ThetaJA so as to not exceed the maximum junction temperature of 150 degC. Tj = Ta + ThetaJA*Pd

    4. This will depend on package and layout: it is shown on page 4 of the datasheet for the different packages.

    5/6. Assuming minimum current consumption, the theta JB and JC value is useless in an application because the temperature rise is insignificant. 

    7. This is shown in the Quality section of the device product page. Weight 26.1 mg