Hello,
i want to design an inverter with 25 to 50V DC input and 250Vrms pure sinewave output with flyback topology with unfolding bridge . The output of flyback should be rectified sinewave. Can i use UCC28950 or maybe UCC2895 to generate rectified sinewave with 100Hz or are they only for DC/DC conversion ?
I don't want to use DSP kits and programming languages because of the limited time. If there are any other controllers that i can use, please reply this post. I will appreciate if anyone can help.
Thank you very much
Semih