Hello,
I am developing with the BQ77910A chip and have ran into some configuration issues. In the data sheet the schematics are slightly ambiguous when it comes to the grounds. The configuration is the same as Fig13. "Example Series FET Configuration Using the CHGST Pin". It seems that the PWR (PGND) ground and REF (AGND) ground make a floating ground relative to the other parts of the system. When communicating with the chip do you make a common ground with PGND and ones Digital ground? I have made a quick block schematic of the power loops that are being dealt with, see attached. I was seeing a large voltage difference between my digital ground and PGND so I wanted to verify the proper I2C implementation before attempting.
Thanks for any help.