Hi, I have designed a SMPS with the following input and output specs and the design is based on TL3844. Kindly let me know if the design is OK.
Input = 20V to 150VDC
Output = 5V at 3 Amps
Operating freq = 40KHz, assumed efficiency = 75%, Max Duty cycle = 0.45(discontinuous mode)
I get a turns ratio of 3, Primary inductance of 315 microHenry,
Primary turns of 72 and secondary turns of 24 (for 5V)
The transformer core selected is EE2005 and a 300V MOSFET is selected. KIndly let me know if the design is OK
TL3844 has max duty cycle of 50% and start up threshold of 16V
Regards
Atul Bhakay