We are currently using a BQ24167 in a design. From what I can gather from the datasheet, the max battery current when no external power is available is 5uA. Unfortunately, we're seeing around 30uA. The only pins that I can imagine would effect this are the IUSB_ lines, but when measured, they are in their intended states to limit the USB current to 500mA. IUSB2 and IUSB3 are both pulled low with a 150k resistor (and are driven by a GPIO from our processor). IUSB1 is connected directly to the DRV output. CE is also pulled low with a 150k resistor (and connected to a GPIO on our processor). What am I missing??