This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Teachers Gentlemen:
National Semiconductor
It is to my liking yet greet cordially ask a small contribution concerning the integrated circuit manual: LM723 / LM723C Voltage Regulator. The maximum output is 30V.
- To amplify 20 volts but I need an amplifier that is the one with blue lines, plus 50 volts would be, would the configuration of transistors is right or not, there is another way and in a serious way.
- A controller as in the case of the red lines 2SB1587, or you do not.
- A power transistor orange lines the MJ15003 140V - 20A
- Transformer 220 / 36V / 5A.
- Regarding the current would vary the appropriate configuration to control the current.
- There is a manual National Semiconductor and the LM723 integrated manual and more, vary the current configuration, could provide me a copy.
- The TL783 integrated can be used as a regulated source, if it had a diagram of a regulated source of 0-50V 5A composed of the same might give me a copy.
- Enclose a copy of the diagram.
- Daniel greetings appreciate your contribution.
Mr Samame,
Are you available to answer a few questions?
Peter
petermpeters@gmail.com