Hello,
I am working on a design which has recently made the change from the BQ500110 to the BQ500210. Everything seems to be working fine except for some unexpected behavior that I'm seeing on the LED indicators (specifically LED1 on the BQ500210). I am using the BQ51013 on the receiver side.
When I place the RX coil on the TX coil, LED1 begins to slowly flash green indicating power transfer. When I force the BQ51013 to terminate the transfer (by pulling TS/CTRL high) then I see LED1 turn solid green.
Then, if I stop forcing the TS/CTRL pin on the BQ51013 high and wait 5 minutes - the power transfer will start again but LED1 turns off and remains off instead of flashing. Once I send another termination packet from the BQ51013 the power transfer will stop and LED1 will turn solid green again.
I have tried LED modes 1, 3, 4 and 5 and they all show the same behavior.
Is there anyway to make LED1 not turn off (it can either remain solid or slowly flash) if a power transfer is re-initiated after a termination packet has been sent?
Any help or information would be greatly appreciated.
Regards,
Dean