This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65250

Other Parts Discussed in Thread: TPS65250

Hi all,

I am using TPS65250 in one of my application with following output requirements,and the Input is 12V/1.5A:

5V/2A on Buck1,

3.3V/1.5A on Buck2 and

1.8V/1.5A on Buck3. 

Sequencing : Vcc first after 10ms 1.8V and 3.3V should come up.

The Gasp time we require is 2.5 S ie. after the power has been shutdown the power should be present for another 2.5s.

Referring to the datasheet "PUMP AND DUMP SECTION" page-29

As per the datasheet it is better to use BUCK-3 in GASP mode as it is closer to Buck-3 Pins and layout will be easy.

My doubt is whether storage capacitors will give the power to buck-3 only( As BSTDG is connected to buck-3) or to two others buck converters that is buck-1 and Buck-2.

Early response will be appriciated

Thank you very much in advance


Thanks and Regards,

Sanjeev Kumar