Other Parts Discussed in Thread: UC3906
Hi All
I am using UC3906 for charging my SLA battery 6V 4.5Ah battery with the following specifications.
Voc = 7.5 V, Vf = 7V, Imax = 500mA (C/5) Vin = ~10.5V, V31 (float to bulk transition) = 6.3 V
The problem I am facing is, the charging time is too slow. it takes more than 24 hrs to full charge the battery and reach float voltage ( I am getting a float volatge of 7.1V practically). As my Imax is 500mA for a 4.5Ah battery it should take 9 hrs to fully charge the battery. By the way, the transformer used is a 9-0-9 1A rating which would be sufficient to provide the 500mA as dictated by using the resistor Rs=0.5ohm
All other parameters are matching my design, except this. Is there anything else I am missing. Please let me know what could be done to resolve this problem
Regards
Ananthu