This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a test PCB using a LM3478 and a design from WEB-BENCH , I am not getting any switching output on the DR pin , this keeps the external Fet ON all the time, I have 0.7V FA/SD . this is a variable boost circuit ,
I have tried everything I can think of , I removed the Ind, from the circuit to test the switching and have had no luck , New parts all around,
I posted the schematic and Web Bench design below , any suggestions are welcome !!!!
Hi Mike,
I will let the application engineer know to look at this post.
I have a couple questions.
1) What is the component U1 which is tied to the FB trace? Anything connected to the FB node I would check to see if it is holding the pin high which would turn off the switching action.
2) Are you sure that CIN and Cout are oriented like this in the schematic, with the positive side connected to ground? If so, the capacitors might have shorted.
Regards,
Marc
U1 is a AD5228 10k ohm digital pot , I changed R4 to a 4.7 k , and have a range of 0.3 - 2 volts at FB on LM3478 , the caps just drawn wrong , they are ok on the PCB ! ( fixed that )
thanks !
OK as I adjust the feedback by changing the digital resistor value , as the FB pin goes past the 1.26 volts the output from DR changes from 0 volts to .57 volts FYI but never goes into switching mode .
I would try taking out the digital pot and add wirewound lower resistor. If the part works with this then we will try getting the digital pot working. If the part still doesn't work at least one thing is off the possibility list.
Also, what input voltage are you currently using to test the part with?
Marc
Hi MArc , I thought the same thing , I am using a Li-ion battery 3.7 volts Nom. , I will try replacing the Digi pot with a fixed res. I do not have any Wirewound ones just SMT types .
I assume the DR pin should OSC with or without a load correct ?
OK I tried 2 3.3 k ohm res for the feedback R's Fb1- Fb2 same results no switching ! lost here
how does the circuit look >? I could not find any errors
Hello Mike,
that's a simple issue that can easily be solved just by increasing the current limit of your input power supply and please introduce an input filter on your VIN pin like in the following image:
The reason why that happens is:
The LM3478 is low side N-Channel MOSFET controller which is able to reach a 100% duty cycle.Unfortunately, the LM3478 gate driver could gets stuck generating a high driver signal that keeps the MOSFET turned on all the time when the IC hits 100% duty cycle if the input power supply is current limited. Indeed a user should set the current limit of the input supply based on the output current at the minimum input voltage.
The problem occurs because the LM3478/88 doesn’t have an Under Voltage Lock Out circuit which turns off the device when the input voltage goes below a certain value.
Without the UVLO the device will keep switching as long as the input voltage is higher than 2.97V (minimum input voltage). If the customer has set the maximum input current for an input voltage higher than 2.97V what happens is that the input current value will be higher than the maximum allowed at the start up causing the input current limit. When the input power supply goes in current limit, the output of the converter decreases then the duty cycle will increase because the device is trying to get more energy from the current limited input supply. Consequently, the low output voltage will cause the error amplifier to generate a high signal which doesn’t allow the intersection with the sense signal and then turning off the MOSFET. Furthermore the sense signal is no longer a ramp due to the current limit of the input power supply (the input power supply is current controlled instead of voltage controlled). This will cause the device to reach 100% duty which is basically a short circuit at the input.
Thanks , I have a few questions ,
1,. I am testing this under a NO LOAD condition with a Li-ION battery that has about a 4 amp current capacity
2. UVLO is something I will need ! , is there another device that incorporate the UVLO ?
3. the device in this design uses a single Li-Ion battery and has VERY limited PCB space 1"x.8" size so space is limited
I am burning up components right now with no load , is this a normal condition ??? if so I need to change parts for a UVLO circuit.
Hello Mike,
please see my answers:
1.there may be some inrush current causing that problem or something in your set up. Furthermore 4amp are not enoug for a 5V@3A with 3V at the input. I am sure that a big bulk cap should solve the problem.
2. I really encourage you to use the LM3481 inplace of the LM3478. The LM3481 is an improved version of the LM3478 and it implements UVLO that you can set.
3. I would like to take a look at your PCB layout for a quick review.
Anyway please use the LM3481 instead of the LM3478.
Regards,
Giuseppe
Hello Mike,
in any case I encourage you to use the LM3481 instead of the LM3478.
Anyway I took a look at your PCB and schematic.
It is suggested to have a bypass cap (like the one used to solve the previous problem) right on the VIN pin.
Furthermore you should move the C3Csense right on ISEN pin (between ISEN pin and GND) for a better current filtering.
Also please consider the following suggestions for an optimized PCB layout for a boost converter:
FILTER CAPACITORS
Place CBYP as close as possible to the VIN pin and GND pins of the LM3478
Place CSN as close as possible to the ISEN pin and GND pins of the LM3478
SENSE LINES
The current sensing circuit in current mode devices can be easily effected by switching noise. This noise can cause duty cycle jitter which leads to increased spectral noise. RSN should be connected to the ISEN pin with a separate trace made as short as possible. Route this trace away from the inductor and the switch node (where D1, Q1, and L1 connect). For the voltage loop, keep RFBB/T close to the LM3476 and run a trace as close as possible to the positive side of CO. As with the ISEN line, the FB line should be routed away from the inductor and the switch node. These measures minimize the length of high impedance lines and reduce noise pickup.
COMPACT LAYOUT
The most important layout rule is to keep the AC current loops as small as possible. In a boost regulator the primary switching loop consists of the output capacitor, diode and MOSFET. Minimizing the area of this loop reduces the stray inductances and minimizes noise and possible erratic operation. The output capacitor(s) should be placed as close as possible to the diode cathode and the ground side of RSN.
GROUND PLANE AND VIAS
A ground plane in the printed circuit board is recommended as a means to connect the quiet end (input voltage ground side) of the input filter capacitor to the output filter capacitors and the PGND pin of the controller. Connect all the low power ground connections directly to the regulator AGND. Connect the AGND and PGND pins together through a copper area covering the entire underside of the device. Place several vias in this underside copper area to ground plane. If a via is needed to connect the sensing resistor to the ISEN pin, then place that via in the inner side of the sensing resistor such that no current flow occurs. Place several vias from the ground side of the output capacitor(s) to ground place, that will minimize the path for AC current. The PGND and AGND pins have to be connected to the same ground very close to the IC. To avoid ground loop currents attach all the grounds of the system only at one point.
Here an example:
Regards,
Giuseppe