Hello,
I bought a TPS54618EVM-606 Evaluation Kit. I changed the resistor R9 to 33kOhm and R10 to 10kOhm to get a output voltage of about 3.3V.
When I now power up the DC/DC I only get about 2.4V and the VSNS is about 0.5V (not 0.799V). The PowerGood Output is high (that means everything is OK).
At the first try I started the kit without a load. Can this damage the chip?
I checked the resistor values double and triple and I also checked there are shortcuts or something else. But everything looks good.
Have anybody some hint for me?
Regards,
Stephan