Hello all,
I am verifying a design with the BQ24230 li-poly power path management IC.
The charger works fine but when there is a faulty battery pack or no battery pack at all connected to the sytem the BQ24230 goes limp.
There is no power good when the USB is connected and the output voltage of the IC is about 1.7Volts while the input is 4.9Volts (standart USB connection).
Does anyone have any clue why this is?? I allready checked the Iset and Ilim values and they are both set just below 500mA.
Best regards,
Pepijn