Dear,
I am using TPS61221 in the typical application. The circuit is shown below.
Vin=1.5V and Vout=3.3V. In my application, Iin=8.4mA, Iout=2.8mA. So the efficiency is 73%, which is much lower than that shown in Fig3. of the datasheet (about 85%).
I want to know what the possible reasons of it and how I can improve the efficiency of the chip.
Can any one help me? Thank you!