Hi. I'm currently designing a 12v from 48v circuit. I bought "WEBENCH BUILD IT BOARD LM5576" and other components from digi-key. values and digi-key part numbers are on the attached excel sheet
6886.LM5576 12v design.xlsx
the input power is connected via a RJ45 connecter. and the load is a resistive test load of about 8.9Ohms (draw almost 1.33A). I assembled 6 boards and ran two of them very well for about 15 hours but then when i plug out and in the power they started to fail all of them. the failure is that the input becomes shorted and the input impedance become less than 10 Ohms. I tried to replace the IC for one board and the input impedance become several mega Ohms but when i plug power in the same problem occurred again.. I'm so confused. do you have a clue? is there an important notes I should be more careful about?