Hellow,
the data sheet of the bq78pl114 refers always to calibrated devices if terms related to accuracy. So calibration is demanded.
How is it possible to calibrate the bq78pl114 with bq76pl102 in an industrial manner without the need of artisan bqwizard usage?
Can we for example produce the calibration file by supplying 2800mV, reading all voltage readings, supply 4200mV, reading all readings again, calculate a little and write the results to the calibration file and this file into the bq78pl114?
Or is it possible via SMBus? There we need the registers and calculation etc.
Or other or more simple solution?
Best regards
Andreas