For LP3852EMP-3.3 (SOT-223-5) I can't find answers to either of the following two questions in the datasheet:
1) What is the over temperature protection shutdown threshold temperature. (degrees C)
2) What is the theta ja for the SOT-223-5 package.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For LP3852EMP-3.3 (SOT-223-5) I can't find answers to either of the following two questions in the datasheet:
1) What is the over temperature protection shutdown threshold temperature. (degrees C)
2) What is the theta ja for the SOT-223-5 package.
1) Thermal shutdown is typically at 160°C. This threshold is characterized prior to RTM only. This is not production tested, or a guaranteed line item. Thermal shutdown is outside the Guaranteed Operating Range.
2) Theta(j-a) is estimated to be 145°C/W