This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB Device Not Recognized using AM3703CUS with TPS65930

Other Parts Discussed in Thread: TPS65930

Hello,

I am trying to erase the MT29F4G16 Flash using your Flash v1.6.0.0 program. I am successful using the RS232 UART. But I am not successful when I select USB. My set-up is as follows: My target is AM37xx (Micron), Memory type is NAND, ONFI compliant is checked, 1-Bit ECC layout Layout X-Loader/U-Boot,  and I am using the TI TPS65930 with ID (pin G6 floating) VBUS connected to USB_VCC. The TPS65930 UCLK (K11) is connected to HSUSB0_CLK/GPIO_120 of the AM3703CUS, DIR (H11) is connected to HSUSB0_DIR/GPIO_121 of the AM3703CUS, STP (H12) is connected to HSUSB0_STP/GPIO_122 of the AM3703CUS, and NXT (J8) is connected to HSUSB0_NXT/GPIO_124 of the AM3703CUS. When I power I get “USB Device Not Recognized”. Any suggestions? Cliff