This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Maximum battery capacity of BQ2060A

Other Parts Discussed in Thread: BQ2060A

We are going to develop a 20Ah Li-Ion battery pack and intend to use this IC for this project but we are confusing on the ability of maximum battery capacity.  

From the BQ2060A datasheet , we found that the max. battery capacity is 65Ah as below:

 

From the TI Selection Guide(page 49), we see the following table which stated that the max. battery capacity is 10Ah:

 

Could anyone can tell us if this chip can fit to handle 20AH battery?

Thanks!