Hello.
I have made a new NIMH charger design with the BQ24400. The design is almost like the design example in the date sheet.
The charger shall charge a 3-cell NIMH block. I have chosen Bat input voltage devider as followed R6 200K and R7 160K.
That should give a Cell voltage of around 1.5V.
The problem is that it never stops charging, because it regulates the current down so that i never reaches the cell Voltage of 1.5V.
Can You heltp me out here and may be come up with a design example