This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Data Flash of the b27505.



I'm using the bq27505 with MSP430.

I can't read the data flash of the bq27505.

I tried to read the data of configuration class (subclass ID is 48).

Offset of Device name is 16 in datasheet page 22.

But when I read the data flash, first character of device name start always at 15th offset.

below log is data which I read.

0  : 0x01

1  : 0xB0

2  : 0xF6

3  : 0xFE

4  : 0x0C

5  : 0x03

6  : 0x84

7  : 0x5A

8  : 0x03

9  : 0xE8

10 : 0xFE

11 : 0x70

12 : 0x0B

13 : 0xA6

14 : 0x07

15 : 0x62  'b'

16 : 0x71  'q'

17 : 0x32  '2'

18 : 0x37  '7'

19 : 0x35  '5'

20 : 0x30  '0'

21 : 0x35  '5'

22 : 0x00

23 : 0x00

24 : 0x00

25 : 0x00

26 : 0x00

27 : 0x00

28 : 0x00

29 : 0x00

30 : 0x22

31 : 0x00

I think offset of device name is 15.

Is it right?

Can I get the tips or examples for reading data flash?