This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Doubts related to bq78pl114 configuration files .tmap and .aux.

Other Parts Discussed in Thread: BQ78PL114

Hello,

I'm using a bq78pl114 and I have some doubts about some configuration files that this IC uses.

In application report SLUA495A (http://focus.ti.com/lit/an/slua495a/slua495a.pdf) says in page 1 that the minimum number os parallel cells that we can put in the .tmap file is 1!.

So, in my application, my battery stack is formed by 4 Li-ion series cell, I don´t whant any cell in parallel configuration. Can I put the number 0 in the indicated line of the .tmap file when I open it with the Notepad??How can I work with this situation?

Another thing that I don´t understand is in application report SLUA505 (http://focus.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=slua505a&fileType=pdf). In page 3, 3.2.2 (Aux file) I follow all the instructions, so I choose the 0101_8S1P.aux (example) and I open it with text editor. But I crash again when I try to calculate my pack capacity (my bateries have 90Ah of nominal capacity), because I don't whant to use bateries in parallel and I don't understand where it come the "x1.2" of the example formula that is given for we calculate the Qmax value.

So here my doubts are: in the example given in SLUA505 (2400 x 3 x 1.2 =8640)
-It's mandatory the capacity in mAh?
-x 3 is the number of parallel cells, right? What can I use in my situation?(none cells in parallel)
-what means the x 1.2?
-There are any mandatory relation between the Qmax and Qrem values?What can you suggest?

Best regards,
Brayts

  • For me the minimum of 1 in parallel is a logical value; 1=1 cell, i.e. single stages, 2=2 cells in parallel, 3=3 in parallel etc. To enter zero would mean zero cells in parallel = no cells at all, then you do not need any BMS ;-)

  • PerBear I'm still not understand completly...

    To me series of batteries is something like this:

    (and this is what I want)

    the parallel needs a minimum 2 (batteries in this case), so for 1,2,3,4...etc, the assembly is something like this:


    "To enter zero would mean zero cells in parallel = no cells at all"!! And the cells in series?! You can not use???

    Can you or someone else explain better my questions in the first topic?

    Regards,
    Brayts

  • Hi,
       
    I already understood the meaning of "x1.2" in the example formula "(2400 x 3 x 1.2 =8640)" that is given in SLUA505.

    However I still not understand very well, how can I put a configuration only with series of cells? For pack configuration only with series cells (until 8 for the bq78pl114) in the .aux file and in this formula I only need to use the value 1?

    regards,
    Brayts    

  • Yes, enter a value of 1 in the aux file and in the formula. The terminology for the device for 4 series cells in parallel for example would be 4 series cells and 1 parallel cells, the pack would commonly be described as 4S1P.  The parallel count for the device is 1 although there is nothing extra in parallel with the 1 cell.  The parallel count number used to configure the device is the total number of cells in that series element, not the number of additional cells.

  • dear Brayts,

    when battery manufacturers describe their battery designs for example as 4s1p or 3p9s they mean the following: 4 cells (4s) are put in series in 1 'parallel' string (1p) or 3 cells in parallel, 9 of these cell packs in series. There is no '0p' configuration.

    best regards

    Bernd