sir,
during chemistry learning there are in between steps of relaxing the cells
this relaxing means, disconnecting cells from 1N to 4P, or just the removing charger and load.
becoz if cells are removed, then EVM goes in shut down and learning process breaks, so i hope cells are to be keep connected to evm and remove just load and charger for relaxing
isn`t it?
but in step of learning where it says, pulse discharge from 10% to 3v, it completes the step and goes to step 7 of relaxing , so i remove the load to relax, but again it goes back to step 6 and says EXTRA STEP, pulse dischrge from 10% to 3v requres more time, so i connect again load then it deschages and goes to step 7, but this happens over and over and each time it starts timer from 0, for 5 hrs relaxing, co never completes step 7
pls help
thanks and regards
rohit