Hi, I am trying to get my arms around all the details of the process before implementing the design of a BQ27541 (GG). I've read SLUA504 (Going to Production With the bq2754x) and I understand the testing of samples and creating a DFI. I understand that calibration for each board/circuit is optional at production.
The thing I don't understand is how does the bq27541 (GG) find or know the initial capacity of the cell, when it is first connected to the cell? The cells will vary some on their initial capacity from the cell manufacture as they are installed in the pack with the bq27541. Cells are not shipped at full capacity. Their may be a procedure for this, but I haven't seen yet.
Thanks in advanced,
Wally