This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If you go to the bq2085 V1P3 product folder you will see a link to EVSW
http://www.ti.com/litv/zip/slvc167
is the direct link. Under "Options/Comm Port" you will see a USB option. This will use the EV2300. Be sure you have installed the drivers for the EV2300 prior to doing this. If you have not, do not plug in the ev2300 until lthe drivers are installed. I recommend installing the bq20z80 or later EVSW (you can get it through the website too) which will automatically install the drivers first. Then Plug in the ev2300 and follow instructions. Then install the bq2085 EVSW.