Other Parts Discussed in Thread: LM3478
I am using a modified LM3478 EVAL BOARD to generate 24V @ 3A. It works OK but the external FDS6690A power NFET gets very hot so I don't run it very long. What can be done? Is there a better NFET selection: put some in parallel, add a heat sink, etc? Per WEBENCH recommendations, I'm using:
1. L= 4 uH Inductor DCR=1.94mOhm IDC=25A (CoilCraft: SER2014-402MLB).
2. D1= Vishay VS-30CTH02SPBF
3. Rsn= 0.003 Ohm.
4. Rfb1= 16200 Ohm
5. Rfb2= 1000 Ohm
By the way, it's confusing the way Webench switches the definitions of Rfb1 and Rfb2.