This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS76901-EP and Q1, Set to 3V3 as per procedure but I get 3V0.

Other Parts Discussed in Thread: TPS76901-EP

I have issue with this device.

 

(1) TPS76901-EP quoted internal reference as 1.124V

(2) TPS76901-Q1 quoted internal reference as 1.224V

 

The TPS76901-EP was shipped from Digikey for pre-production qualification test (next year it will be volume production),  

 

I have fitted the TPS76901-EP on board with R2 = 150K and R1 = 249K which provide 3V3 (based on Q1 datasheet). I get 3V0 rather than 3V3 (or 3.26V).

 

I also get 3V0 into 1K load.

 

I build a breadboard with nothing on circuit except the TPS76901 and have 1uF cap on VIN and VOUT. I use VIN = 5V from bench PSU. It confirm 3V0 output for all three devices. The equation in datasheet (Q1) say it should be 3V3 but uncertain which VREF is correct.  

 

I check the FB pin and measured 1.20-1.21V (that with 1K load). (NB: there is possibility of DVM loading effects).

 

In order to make O/P to 3.3V, I adjusted the R1=270K and it seem stable over the load to 50mA.

 

Q1: Is this device defective, has the internal VREF set incorrectly or ?

 

Q2: Can you confirm which is correct VREF voltage between EP and Q1 as this is confusing?