This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi fl, the discharge automation (step 2-4 in the learning cycling screen) through bqEasy is optional.
You can choose not to use the "option" button and manually discharge the pack by following the on-screen instruction. Click "All Done" button when you're done. Upon completion of 2 learning cycles, bqEasy will create the golden DFI.
Regarding the data overflow error, I have sent you an email to ask for more infirmation regarding your project.
Felix,
bqEasy use information in the DFI saved from the previous steps in the process of generating the golden DFI. If those files are missing, you'll error messages and golden DFI will not be created.
Though I saw from your attachment that you have finished Step1 (setup), Step3 (calibration), Step4 (Chemistry), but those check marks can be shown by loading an exisitng .ezy file. Can you cinfirm which steps did you complete?
The 2nd error message could be cause by several things:
1. you have a missing .encr file for the device you're testing or
2. the data flash structure in the device doesn't match with the .encr file that bqEasy is trying to use
3. communication error
The 3rd message is bogus. With error messsage 1 and 2, bqEasy will not be able to generate a golden DFI for you. The future revision of the program should improve the message flow.
In order to asssit you, I'll need more information of your setup and test flow. I tried to send you an email through the your forums profile, but I got an error instead. Can you send me a email through my forums profile, so that we can continue this conversation without explosing too much of your system design?
HI
I have similar problem with bq27500 v130
I am continuous getting an error every time I try to finish the chemistry cycling.
“Error Logging Data: Overflow”
I am using the automated version described in slua544
Can any one help me with this error?
Best regards
Emil
I see this post is from 2010, but I am having the exact same problem as Emil when I finish the chemistry selection cycling then try to write it to the device, I get overflow error and bqeasy crashes and shuts down and I lose my cycling information which is about a 12 hour procedure or so.
My device is BQ27500-V130