I am using the bqEasy program to test configurations of a 12 cell Lion pack. Some registers I can set easily such as "Over Temp Chg" and "OT Chg Recovery". But other registers won't change like trying to set "Chg Inhibit Temp Low" from -10 to -5 or "Rem Cap Alarm" from 300 to 440, or "FET Fail Time" from 0 to 1. When I try to change them the old value comes back in red letters. My application requires the FET Fail function to work. Can I just use PRO mode to force the bytes or is there a good reason bqEasy won't set things as I want?