This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL3844 , 16W SMPS design - Wide Input

Other Parts Discussed in Thread: TL3842, TL3844

Hi,  I have designed a 16W SMPS using TL3844 with a wide input of 20V to 150VDC. TL3844  has a max duty cycle of 50%. Should i have considered TL3842 instead - TL3842 has max duty cycle of 100%.

Attached is the schematic and transformer details of my design. Kindly advise 

2844.TL3844_3 output_EE2507_Transformer_r1.doc

2605.TL3844_ 3 output_EE2005_schematic.doc

Atul Bhakay