I have a requirement to regulate from 100v (max) to 5v, to power a micro and a USB (charge port 500ma)
I have not used or tested the LM5017 before, and I am concerned about ripple from the regulator affecting the micro.
The 100v battery input supply will dip around 4 volts when loaded elsewhere.
Questions
1. Should I regulate directly to 5 volts using the LM5017 (which Type 1,2 or 3 should I use in the design) ?
2. Should I regulate to 12 volts using the LM5017 and then re regulate to 5 volts with a conventional regulator?
3. If the input voltage is 100.3v, will this damage the LM5017? (When fully charged the battery is 100.8v) I can add second diode to drop the voltage by 0.5v when loaded.
Thanks
Andrew