This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ucc28950 thermal problem

Other Parts Discussed in Thread: UCC28950

Hi everybody;

I'm at the beggining of phase shifted and I only gave 15V to 23'th pin of ucc28950 and a GND to 24'th pin. But the tempreture of IC goes up and when I measure Vref pin I see 6.7 V instead of 5 V. Does it need any connection to see 5V or something wrong?