This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is that workable to do LM3478 3.3V input to 5V2A vout?

Other Parts Discussed in Thread: LM3478

Dear sir,

  We test LM3478 EVM board & try to change Vout to 5V2A but can't work. We use both datasheet page2 circult & webench circult  but result is the same.

So is that workable? Or what should we have to know about LM3478 if we need to use on 3.3 input?  Like Vgs threshold or something?

The fail symptom is before 5V 0.2A, sw node is normally but over 0.2A sw node will start jitter & unstable... Output ripple will become larger.