the three 4.7 uF capacitors C2 that are labeled 'Required' with the PTN - these are a little hard to get right now, and I'm wondering if I can use electrolytic capacitors in their place. we need to get our project moving forward fast, and I'm wondering if they have to be ceramic and why, if so. also, does TI sell these kind of parts at all, i.e. external parts required with a TI part?
thanks