This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buck with Dying gasp

Other Parts Discussed in Thread: TPS65250

Hi all!!

Can anyone please suggest a down converter with input of 12.0V and output of 5.0V, that must have dying gasp mode functionality. I referred TPS65250 but it has got three bucks, due to constraint in board size that doesn't allows to add lot of components. single output buck with gasp is needed. 

Or is there any possibility to disable the other two bucks of TPS65250 and use single output in GASP Mode.

Thanks in advance!!!

Best Regards,

-Anand Kumar Rai