Dear Team,
We have got an opportunity of BQ24610 and other BMS parts from Simens.
Please refer to below business status.
- customer : Siemens
- part no : BQ24610 (Battery charger IC)
Battery pack side: BQ29312,BQ2084,BQ29412
- Application : potable ultrasonic waves
- MP : Mar/2013y
- Q’ty : 10k/m
They have got an issue which is sometimes no charging operation.
When they produced 30EA applications, some products are not charging the battery intermittently.
Please refer to below experiment status.
1. input and output specification: Vin:19Vdc, Vout(bat: 4EA):16.8V/3A
2. abnormal status(no charging) :
1) When DC input pulgs in the application W/O batteries, the Battery charger FET is operated very well.
2) When Batteries pulg in the application, sometimes the Battery charger FET switching is abnormal like a OCP.
The phenomenon is occurred intermittently.
Please refer to attachments.
If you need more information or waveforms, please reply it to me.
Thank you.
Best Regards,
Tae Ho