This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power supply for load cell

 Hi,

 one of my customer is working on weigh scale for powering up load cell they are looking for +9VDC and -9VDC

V input DC   :- 20 - 30 DC
Vp-p tolerance should be less the :- 2%
Maximum current :- 1A 

Looking for part suggestion or solution 

Regards,

Datta