Hi,
I am using TPS40057 and added some special current limit delay circuit(used PNP Transistor and RC delay circuit) between Vin and current limit resistor.
It makes about 200ms delay at start up so output voltage does not hiccup even if there is a peak output current over current limit set up during the 200ms.
My question is, while current limit pin opens for this delay TPS400057 is stable or not ? I mean TPS40057 supports current limit pin open? Thanks.