This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

low power isolated DC-DC controllers

Other Parts Discussed in Thread: TPS55010, TPS40210, TPS61175, TPS61170

Hi,

I need controller ICs for the following requirements. Input to output isolation is 3KVdc

Pls suggest.

1. Vin=+/-5Vdc, Vo=+15V & -15V, Io=50mA each ; eff=60%; PARD=100mV

2. Vin=+/-5Vdc, Vo=5V, Io=200mA ; eff=60%; PARD=100mV

3.Vin=9 to 36Vdc; Vo=5.1V; Io=2.35A; eff=80%; PARD=40mV

Thanks.