This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24230 Problems with charging

Other Parts Discussed in Thread: BQ24230

Hello,

I made a prototype board design for the bq24230. The power switching aspect of the IC worked fine, but I had some weird issues with charging. It seemed that the charging rate varied depending on the current battery voltage. For example, with a 5V input source, I get the following: RISet = 15 kOhms Ichg = KIset/RIset KIset = 870 AOhms (typical), 797 (min), 975 (max) Ideally, Ichg = 870 AOhms / 15 KOhms = 58 mA.

However, I get the following, when putting an ammeter through the positive terminal of the battery.

Battery Voltage (V) Current (mA)
3.4 59
3.6 59
3.7 59-60
3.8 60-61
3.85 63
3.9 64-65
3.95 67
4.00 69-70
4.05 75
4.10 77
4.15 79
4.18 60
4.185 50
4.19 40

I would appreciate any helpful feedback.  Thanks in advance.

Sincerely,

Mehdi

  • So it turned out that the problem was not having sufficient capacitance on the battery line.  When I placed a 10 uF capacitor on the battery line, the charging current stabilized to ~58 mA, and the chip worked as expected.  Silly mistake on my part, but glad I found the issue.