This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65950 powering issue

Other Parts Discussed in Thread: TPS65950, DM3730

Hello!

we are using PMIC TPS65950 with DM3730.

As per PMIC datasheet, maximum current on VPLL1 rail is 40mA. VPLL1 provides power to two processor rails:

  •  vdda_dplls_dll (30mA maximum current).
  • vdda_dpll_per (10mA maximum current).
Is PMIC power rails capable of supplying power at temperature (-40C to +85C)?
Or is there any restriction?
Thanx in advance.