We designed 5S 2P Li-Ion Battery pack with BQ34Z100 Gas Gauge and BQ77910A Protector. We got the design verified by Local TI. We have tested for charging, discharging, short circuit current, battery cut-off, etc.,
Now, we are facing below described problem and looking for clarification on few questions
- What is the advantage of using FET switch in Batt- instead of Batt+?
- Usually, power disconnect means, +ve / Phase terminal to be disconnected instead of –Ve / Neutral line. Right? But, in this case it is –Ve.
- Now, our specific problem is.
- Since, we are not disconnecting Batt+ terminal, the voltage appears till our DSP TMS320 after battery cut-off at 15.5V. Due to which, the battery gets closed path for current through I2C line. Under this condition, we observed 33mA is flowing out of battery which causes battery to drain further. We disconnected the I2C line and found no current flows (hardly, 0.3mA).
Kindly provide us the solution for this issue.
Further, in BQ34Z100’s datasheet, page no 4, figure 2 depicts that FET switch to be used on Batt+ terminal. How it is feasible with BQ77910A as it got N-channel driver and other connections required for driver (CCAP, CPCKN). We are confused with the signals to use P-Channel FET switch in Batt+ line. Kindly clear us. Hope, Using FET switch in Batt+ solves the issue we are facing.