This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Please recommend a standalone switch mode charger for sigle cell handset application

Hi,

   I'm looking for a charger for my handset. The requirements are:

   1.standalone with switch mode;

   2.single mini-USB input compatible with USB(100mA) and AC/DC adapter(1A);

   3.be compatible with common cellphone adapter, the current may be larger than 1A;

   4.can display the status(1)in charging (2)finish charging.

   The simpler to use, the better.

   Thank you!