Hi,
I did a webench design with the LM3150 and noticed that the FETs were only rated at 30V. My design requires up to 36V. Can the LM3150 drive higher voltage fets such as the CSD18502Q5B. Is the 30V a restriction of webench or of the controller? It also looks like the current never actually goes through the controller. Does this mean that I can use it in higher current applications (assuming I use the correct FETS and inductors)? Assuming I can drive larger FETs for higher voltage/current applications, would switching effects become an issue?
Thanks,
Geovid Kali