I need to boost 3V to 20V, but only need <1mA of current. I need a very small solution for my portable device. Most boost converters I find seem to not operate at at very low output currents.
What would be the best way to generate <1mA at 20V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need to boost 3V to 20V, but only need <1mA of current. I need a very small solution for my portable device. Most boost converters I find seem to not operate at at very low output currents.
What would be the best way to generate <1mA at 20V?
All of the TPS61xxx boosts operate down to no load just fine. Would the TPS61041 work for you?
I don't see any info about minimum output current, but the efficiency graph doesn't go below about .4 mA. Are we sure it works that low?
I'll explain the application a little more. I'm using this in a constant current source 1-100uA with 20V compliance. The current will be pulsed for 1-2 ms every 100-1000 ms (<2% duty cycle). I may power an opamp with the 20V also, but the total current will still remain below 1 ma. The size and efficiency of this is extremely important, as it will be used on a small battery powered device.
Yes, it operates down to no load just fine. There is a whole family of TPS6104x devices with various features that might make your design a little easier.