Hello All,
I have prototypes of a LM5574 design that has 7 - 41 V input and outputting 3.3 Volts. (I used WebBench to design it) It appears to be converting OK, but when I look at the recirculating diode side of the inductor with a scope I see small spikes (about 5 volts peak) between the square waves and was wondering what would cause this? I have a LM5574 eval board and it doesn't appear to have these spikes. Any ideas what is causing this or how to mitigate? The device I am powering pulls from 20 - 250mA.
Thank you
Brian